Tripp Lite
1111 W. 35th Street
Chicago, IL 60609
+1 (773) 869-1776
+1 (773) 869-1329
presaleshelp@tripplite.com

How to Reset a Console Server's Factory Default Settings

A factory reset will reset your console server back to its original factory default settings. The IP address will reset to 192.168.0.1.

There are three ways to reset the console server to factory defaults:

  1. Use the Web console.
  2. Use the Erase button.
  3. Use the command line.

  1. Use the Web Console

    Check both Config Erase and Reboot in the SystemAdministration menu and then click Apply.

    web console reset

  2. Use the Erase Button

    Use a ball-point pen to depress the recessed Erase button:

    • Depress the Erase button twice within a 2 second period.
    • Depress the button while the unit is powered ON.
    • Depress the button gently.
    Note: Do not use a graphite pencil.

  3. Use the Command Line

    To perform a factory reset from the command line, type flatfsd -i
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
We're always available to help with questions, including product selection, sizing, installation and product customization. Call us at +1 (773) 869-1776 or email presaleshelp@tripplite.com.